FAQ

System Alarm when disk not full

FAQ Question A few minutes after starting up my IGSS system by pressing the IGSS Starter icon, I suddenly receive the following System Alarm: But my disk is not full. What’s the cause of the alarm? Answer To remove the popup Alarm box acknowledge the Alarm.   The System Alarm can also be triggered if there is no access

System Alarm when disk not full Read More »

SQL Server installation problems on Vista

FAQ Question I get the error “Failed to compile the Managed Object Format” when the IGSS installer reaches the SQL server installation. Answer This turns out to be related to a corrupt WMI repository – and the fix is quite easy. Run the following commands in the C:Windowssystem32 folder. C:Windowssystem32>winmgmt /verifyrepositoryWMI repository is INCONSISTENT C:Windowssystem32>winmgmt

SQL Server installation problems on Vista Read More »

Sql Server express

FAQ Question I Can’t find Sql server express in the installation files for my IGSS Version 9? Answer We have decided to decrease the size of the installation files, but the SQL server express is free ware and can be downloaded here: http://www.microsoft.com/sqlserver/en/us/editions/express.aspx

Sql Server express Read More »

Slow Operator station

FAQ Question  Why is my IGSS operator station slow to react when I right-click on an object? It takes a long time before the object menu opens. When I right-click the same object on the IGSS server, the object menu opens immediately. Answer The Maintenance Module has probably not been disabled for the operator station.

Slow Operator station Read More »

Sinec H1 connection failure

FAQ Question Why does my Sinec H1 connection fail with error code 1202 after updating from IGSS version 8.x to IGSS32 v3 Answer After updating from IGSS version 8.x to IGSS32 v3, one or more of the Simatic S5 PLCs connected to the SINEC H1 network will no longer connect to the IGSS32 server. An

Sinec H1 connection failure Read More »

Siemens TC35i – adding new commands

FAQ Question I’m having problems with my Siemens TC35i GSM modem. I couldn’t find this modem under the WinPager menu Service Providers – List of Services so I chose the one called Siemens M20/MC35/TC35 Terminal for dial out and the Dial-in (Siemens M20/MC35/TC35) instead. I use the same modem for both dial-in and dial-out. Alarms are dialed out to my cell

Siemens TC35i – adding new commands Read More »

Scroll to Top