FAQ

Sinec H1 connection failure

FAQ Question Why does my Sinec H1 connection fail with error code 1202 after updating from IGSS version 8.x to IGSS32 v3 Answer After updating from IGSS version 8.x to IGSS32 v3, one or more of the Simatic S5 PLCs connected to the SINEC H1 network will no longer connect to the IGSS32 server. An […]

Sinec H1 connection failure Read More »

Siemens TC35i – adding new commands

FAQ Question I’m having problems with my Siemens TC35i GSM modem. I couldn’t find this modem under the WinPager menu Service Providers – List of Services so I chose the one called Siemens M20/MC35/TC35 Terminal for dial out and the Dial-in (Siemens M20/MC35/TC35) instead. I use the same modem for both dial-in and dial-out. Alarms are dialed out to my cell

Siemens TC35i – adding new commands Read More »

Sequential reports not viewable

FAQ Question When I want to create sequential reports and select View to preview on screen, I can only see one of the reports in the sequence, the first. Why can’t I see the remaining reports? Answer View is only able to display the first report in the sequence. However, when you select Print, all the reports in the

Sequential reports not viewable Read More »

Screen refresh too slow

FAQ Question When I close a picture/diagram on my PC, which is an operator station, it takes several seconds before I can again see the screen to perform other tasks. How can I speed this up? Answer All pictures and graphics are stored in a device dependent format to make screen updating or refreshing occur

Screen refresh too slow Read More »

RMS on network drives

FAQ Question I get an error when trying to run an RMS report from a shared network drive. Answer RMS reports cannot run if the templates are located on a network drive. Windows security does not allow for add-on applications to Excel, like RMS, to run from network locations.

RMS on network drives Read More »

RMS Action Pane missing

FAQ Question I create a new RMS report, but the RMS Action Pane is missing in Microsoft Excel. Answer This problem may be caused by various reasons: 1. Wrong version of Microsoft Office       The following Office Editions do NOT work with RMS      (because these versions do not support Microsoft VSTO).     Microsoft Office Small

RMS Action Pane missing Read More »

Scroll to Top