FAQ

Using symbol libraries in IGSS

FAQ Question Can I use any symbol libraries other than the built-in IGSS symbol file, Symbols.v12? Answer Many of our competitors use the symbol library called Symbol Factory. It contains a number of drawings well-suited for automation systems. The drawings can be exported to *.bmp or *.wmf format (*.wmf is recommended for IGSS32). Once converted,

Using symbol libraries in IGSS Read More »

Using IGSS32 User Administration

FAQ Question How do I deploy password security and object protection in IGSS32’s User Administration? Answer There are many possibilities for deploying User Administration in an IGSS32 configuration. An overview of various scenarios are contained in the following documents. For English you should download the document  igssuser.doc  and for German igssuser_deu.doc. Each document contains 10 examples, which

Using IGSS32 User Administration Read More »

Transparent symbols not wanted

FAQ Question Why are the symbols transparent on the process diagrams when my configuration is running? Answer Symbol masks can be shown transparently. This means that the background colour becomes visible through the symbol. Transparent is the default setting and this affects the visual appearance of the process diagram, which may confuse operators used to

Transparent symbols not wanted Read More »

Thin Client VBA Error

FAQ Question I’ve successfully installed a thin client solution with IGSS. However, when I start my IGSS configuration up, I get an error message telling me that the VBA code in the configuration failed to load. How can I remedy this problem? Answer To remedy the problem, you must modify two branches in the registry

Thin Client VBA Error Read More »

Scroll to Top