FAQ

IGSS cannot find my printer

FAQ Question When generating an IGSS report (Snapshot, Periodical or Alarm Statistics), I get the message “Failed to render the report. Make sure you have a printer defined in your system, and sufficient memory and disk space”. This happens both when I’m trying to print or preview the report. Answer The message is misleading. The

IGSS cannot find my printer Read More »

If PLC driver doesn’t start

FAQ Question When I start my IGSS configuration or application, I get an error message informing me that my driver won’t start. What should I do? Answer You should begin by trying to activate the PLC driver in question manually. Carry out the following steps: Shut down all IGSS applications and utilities that might be running.

If PLC driver doesn’t start Read More »

If Alarm printer is sticky

FAQ Question If the Alarm printer is sticky and will not let go of my old printer, what should i do? Answer You will need to delete the keys below ”registry HKEY_CURRENT_USERSOFTWARESchneider ElectricIGSS32V12.00.00alarm32_HKLMPrinter name HKEY_CURRENT_USERSOFTWARESchneider ElectricIGSS32V12.00.00alarm32_HKLMPrinterDevMode

If Alarm printer is sticky Read More »

HLVDD.dll not found

FAQ Question I’ve installed my IGSS. But when I start the IGSS software, I get a warning message: ” This application has failed to start because HLVDD.dll was not found. Re-installing the application may fix this problem.” I’ve tried re-installing, but this doesn’t help. I am running Windows XP. How do I solve this problem?

HLVDD.dll not found Read More »

Scroll to Top