Answer
You can do this by setting the following parameter in the Registry:
HKEY_CURRENT_USER\Software\7-Technologies\IGSS32\V8.00.00\DefRun32_HKLM\ShowOnlyTypeSpecPages
If you set this parameter to 1, the object property interface will have a reduced number of tabs, only showing the most basic properties.
You must set this parameter manually on each of the stations where you want the reduced object property interface in Supervise.