FAQ

InstallScript engine missing

FAQ Question When installing IGSS version 8.0, you get the error message below. Answer This error means that the IGSS installer wasn’t able to put the InstallShield 8 engine in the C:Program FilesCommon FilesInstallShieldDriver8 folder. The common reason for this is that you have the InstallShield 1150 engine installed. This will override any attempt to […]

InstallScript engine missing Read More »

IGSS version number naming

FAQ Question How do I interpret the IGSS version numbers I see when I right click on an IGSS program or utility and then go into the Version tab on the right click menu? Answer IGSS version naming occurs as a whole number followed by three decimal points. The first two decimals are not presently

IGSS version number naming Read More »

IGSS V8 Update crash

FAQ Question When I run the update program for IGSS version 8.0, the update program stops functioning and closes, how can i solve this? Answer One of the reasons for the update program’s failure could be insufficient access rights to the DMYREP.MDB file. To find out if you have insufficient access rights to the DMYREP.MDB

IGSS V8 Update crash Read More »

IGSS Update server address error

FAQ Question When I activate the new IGSS v.5.1 IGSS Update it fails with an error: “Server address not found in configuration”. What must I do to remedy this? Answer The server address is not correctly created during the installation of IGSS Update software. Please do the following: Download the zip file found on this

IGSS Update server address error Read More »

IGSS Update Fails Without Warning

FAQ Question I’ve tried to update my IGSS software by using the IGSS Update utility present in the IGSS software package, which automatically connects to the 7-Technologies server via the Internet and downloads the latest IGSS program updates. Every time I try to run the update, however, it suddenly terminates without warning. How can I

IGSS Update Fails Without Warning Read More »

Scroll to Top