FAQ

Portal Graphics Missing

FAQ Question After I log on to the IGSS Portal in my web browser, I’m missing the header bitmap and some of the buttons in the menus underneath. What has gone wrong with my installation? Answer You have probably installed Windows updates somewhere along the line, either before or at some time after you installed

Portal Graphics Missing Read More »

Portal Error Message

FAQ Question I’ve done a successful installation of the IGSS software and the IGSS Portal software on my IGSS server PC. Everything functions perfectly except access to the process I want to control via the Portal. Every time I try to get to the process via the Portal, I get the error message ‘Server Application

Portal Error Message Read More »

Polish version of IGSS Portal

FAQ Question When I activate the settings in the Windows registry (HKEY_LOCAL_MACHINESOFTWARE7-TechnologiesIGSS32V6.00.00IgssPortalAlwaysUseServerLanguage 1 to have the Portal use the same language as the primary language chosen in the System Configuration module on the Supervise & Language tab, I don’t get the Portal displayed in Polish, which is the language I chose. Instead I get the “Page not

Polish version of IGSS Portal Read More »

OPC server registration fails

FAQ Question When trying to register the IGSS OPC server from the server configuration tool you get the error that opcproxy.dll cannnot be found.  Answer This problem occurs because the OPC Core Components are not installed on your PC. You can either download and install the Core Components from the OPC foundations homepage or install

OPC server registration fails Read More »

Scroll to Top