Answer
In GSST log file
ERROR C1010323 GENERAL -1 4996 4888 .\logfile.cpp (152) Allocation of memory failed, memory size requested 67108864, rc = Not enough storage is available to process this command. (0008)
Click on the following link To FIX the ERROR;
“Optimizing LOG file memory allocation in IGSS”