FAQ

OPC Issue

FAQ Question After I have updated my IGSS program, I experience “problems” with the OPC data and I can see the OPC server is still running, even when I restart IGSS after the update, what should I do? Answer When the IGSS update process is initiated, all program elements of IGSS are usually shut down […]

OPC Issue Read More »

OPC Errors with XP SP2 DCOM

FAQ Question I’ve been using OPC clients and servers with my IGSS installation on a Windows XP platform without any problems until now. However, after installing Service Pack 2, my OPC communication no longer functions properly. How do I solve this problem? Answer The Microsoft Windows XP Service Pack 2 has most likely been installed

OPC Errors with XP SP2 DCOM Read More »

OP Station Allowed to Upload

FAQ Question I have been running IGSS32 v4.1 update 1 (build no. 2283) where I don’t want operator stations to be able to see the upload-download dialog box every time a change is made to the configuration. Preventing operator stations from uploading a configuration to the IGSS server was activated on the op station by

OP Station Allowed to Upload Read More »

ODBC Server error message

FAQ Question I’ve been working with my IGSS configuration without any problems. But now, every time I start up I get an error message telling me that something’s wrong with my ODBC server. How can I remedy this? Answer The probable reason is that the IGSS version 5 ODBC server software has somehow been removed.

ODBC Server error message Read More »

New display of Alarm logs

FAQ Question Is there any improvement to the Alarm log list? Answer The Alarm log list functionality has been improved when you update your IGSS application. Previously, if the alarm log list contained records greater than the maximum number of alarm logs, only the most recent (newest) 10,000 alarm logs were displayed in the Alarm

New display of Alarm logs Read More »

Scroll to Top