FAQ

ERW Values Not Generated

FAQ Question I can’t seem to generate any data for the “Previous value” reduction type. What is the cause of this? Answer An error occured when compiling the ERW program to version 3, update 5 (build 2107). This problem is rectified in the patch below, which must be downloaded and copied to the [IGSS installation]ERW […]

ERW Values Not Generated Read More »

ERW patch v.16 triggers an error

FAQ Question When I click the button “Load Config. Objects” or “Bind worksheet field(s)”, I get an error from MS Access. Why? Answer ERW version 16 triggered an error under the following conditions: In the dialogue named “Object selection”, clicking the button “Load Config. Objects” results in an MS Access error message. In the dialogue

ERW patch v.16 triggers an error Read More »

ERW error in Office XP

FAQ Question I’m unable to preview, print, export to Excel or export to HTML when I want to generate an ERW report. I’m working on an Office XP platform and I get the following error message: What must I do to remedy this? Answer Because the problem is in the Microsoft XP Office environment, the

ERW error in Office XP Read More »

Error initializing VBA

FAQ Question I get the error “Error initializing VBA (hr= 80040562)” when trying to start Definition. Answer This error occurs because the dc.exe module is not registrered correctly in Windows Vista when installing IGSS. You can register dc.exe correctly by following this procedure. Log into Windows Vista as an administrator. Open a command prompt. Enter

Error initializing VBA Read More »

Scroll to Top