Answer
There have been minor flaws in the ERW module which have been corrected in the patch below. In addition, the following improvements have been made:
- Command line interface: now, spaces in file names and paths are supported.
- Report generation performance: reduced time for report generation.
- Excel behaviour: by default the Excel workbook is now kept in the background.
The patch consists of two files, ERW.mde and msacsupp4.dll. The first must be unzipped to the [IGSS install path]\GSS\ERW folder and the second must be unzipped to the [IGSS install path]\GSS folder.