FAQ Question
I’m unable to preview, print, export to Excel or export to HTML when I want to generate an ERW report. I’m working on an Office XP platform and I get the following error message:

What must I do to remedy this?
Answer
Because the problem is in the Microsoft XP Office environment, the solution is to download the attached Microsoft OCX file below called MSCAL.OCX, copy it to the folder containing Microsoft Office OCX files and then register it with the regsvr32 utility. Follow precisely the steps below.
- Use the Windows Search to find the default MSCAL.OCX file. There are most likely several files with this name. IMPORTANT: The one to be replaced is located in a sub-folder under the Microsoft Office folder, which is called Office10.
- Unzip the MSCAL.zip file and extract to and overwrite the existing MSCAL.OCX in the Office10 sub-folder.
- Start a command prompt and type regsrv32 [Office10 path]\MSCAL.OCX
- A successful installation results in the message: DllRegisterServer in mscal.ocx succeeded.