FAQ

Alarms to Stationary Phones

FAQ Question How do I dial out an alarm to a stationary telephone? Answer The setup proceedure to have WinPager dial alarms out to a stationary telephone are exactly the same as for fax. The WPMapi service is used and instead of a fax number, the stationary telephone’s number is keyed in. See FAQ number […]

Alarms to Stationary Phones Read More »

Add External types in sysconfig

FAQ Question I would like to change my External types EG to include BCD16 – Binary Code Decimal (16bit) and BCD23 Binary Code Decimal (32bit) but every time I set the checkmarks, the settings are is not saved – why is this? Answer The settings you are trying to save are saved in the local machines registry

Add External types in sysconfig Read More »

Scroll to Top