Active profile only visible profile in list

FAQ Question

I configure a new driver profile in Driver Setup and set it as active. When I do this, my other driver profile(s) disappear from the list so that I’m left with none. If I remember the name(s) of the other profile(s) and re-enter these as new profiles, then they again appear with all the settings I originally used. How can I solve this problem? 

Answer

The problem should be solved by downloading and installing system Update 4.

Scroll to Top