Answer
You might want to remove these entries from the alarm log.
This can be done using the command line tool ALMremoveNum.exe – located in the GSS folder
The commands are: ALMremoveNum folder almno
This removes listed alarm numbers from all alarm files in the specified folder.
Several alarm numbers can be given as a space separated list. The original files are backed up with extension *.aol.
Example:
ALMremoveNum c:\report 1012 1013 1014
Will remove all alarms with alarm number 1012, 1013 and 1014 from all *.alm files in the folder c:\report