FAQ

How to change IGSS Update Service

This is how you can change IGSSUpdateService.exe in IGSS 1. Download the IGSSUpdateService for the version you need below.2. Stop the IGSSUpdateService.exe3. Copy the newly downloaded IGSSUpdateService.exe in to the GSS folder under the IGSS installation and overwrite it. (Administrator rights are required)4. Start the IGSSUpdateService.5. Run IGSS Updater and update IGSS. Download Updater V16 […]

How to change IGSS Update Service Read More »

Running IGSS silent install

FAQ Question How can I run an IGSS Silent install? Answer Windows should have the .Net Framework 4.6 installed. That must be done in the Windows “Apps & features” settings run the installer VSTOvstor40.exe   add /q to make it quiet VCredist\vcredist_x64.exe /q VCredist\vcredist_x86.exe /q VCredist\vcredist_x86_vs2012_110.exe /q msiexec /i  vbacorevbaof11.msi /qb msiexec /i  vbacore1033vbaof11i.msi /qb msiexec

Running IGSS silent install Read More »

Scroll to Top