S7 1500 and IGSS
When using the Siemens S7 1200/1500 series PLCs with the IGSS installation, important parameters must be set in order to address the PLC data registers from IGSS and to read and write to and from the PLC data registers. The Siemens PLC should be set up as follows: Addressing the PLC registers Clear the Optimized block […]