schneider_LIO_White_CMYK

Renaming of areas causes ODBC driver to crash

FAQ Question

I’m trying to rename an area either in the SUPERCONF or the CONF table, but the ODBC driver crashes. Why?

Answer

The above problem has been solved in the attached patch to the ODBC driver. The patch consists of two files:

  • Odbcixv4se.exe (the ODBC driver)
  • AccCtrl4.dll (the Access Control DLL)

Both files must be extracted to the [IGSS InstallPath]\Gss folder.