Missing states and/or command atoms on digital object

FAQ Question
The Definition module (DEF.EXE) generates an error when I open the Symbol tab in the Properties dialogue for a digital object. What is wrong?

Answer

This error occurs when the only atoms defined for the digital object are alarm atoms. Digital objects must also have atoms defined for commands and states.

The problem is resolved in an update of the file DEF.EXE, which is included in system Update 4. Download Update 4 and install it and you should have no more trouble with errors in this context.