I want to print the Note attached to the alarm with my Alarm list but it doesn’t print. And sometimes I don’t get a correct set of columns from the Alarm list on my print out. How can I remedy these problems?
Answer
The solution is an update of the ALM.EXE file, which is available in system Update 4.
Download system Update 4 and install it and the problem should be solved.