schneider_LIO_White_CMYK

Getting help on the ODBC interface

FAQ Question

I’ve read that IGSS features a versatile ODBC interface, but how do I find out how to use it?

Answer

The IGSS ODBC interface is described in the Interface Help file. The help file contains documentation of all the data and programming interfaces supported by IGSS.

To find the ODBC documentation, do the following:

  1. In the Igss32 3.0 Start menu, choose the Interface Help icon.
  2. On the Contents tab, open the ODBC book.