I have objects on underlying diagrams and these diagrams are referenced from buttons on the overview diagram. I need to display some of the alarms originating from objects on underlying diagrams on the overview diagram and I need to hide some of these alarms. Can I do this in some way?
Answer
Yes, it is possible to hide some of the alarms and display others. You can read the news article about Hiding alarms in IGSS (link here)