| Annotate |
Attach your own comments to a Help file. When you save the annotation, a small paper clip appears in the topic. |
| Copy |
Copies the text you have selected in the Help topic. |
| Print Topic |
Prints the current topic. This function is especially useful for What’s This? help topics which are not visible on the Contents tab or in the Index. |
| Font |
Allows you to change the font size. Very useful if you have to read a lot of text on-screen. In that case, change the font setting to “Large” |
| Keep Help on Top |
Determines how the Help file behaves in relation to the program from which it is called. Normally, “Default” will be OK, but if you want to force the Help file to stay on top or remain in the background, this is also possible. |
| Use System Colors |
Allows you to use the colour setup from the Control Panel for the Help files. By design, we have tried to show different information types with different colours, so we do not recommend using this function. |