Update

Security Notification: WSP and CGF vulnerabilities fixed in v15

Thanks to the independent researches Michael Heinzl and the researcher Kimiya working with Trend Micro’s Zero Day initiative the IGSS team has become aware of security issues concerning import of Workspace files (WSP) And Configuration Group Files (CGF) to the IGSS Definition module in IGSS V15.0.0.21041 and prior versions. An update has been released to […]

Security Notification: WSP and CGF vulnerabilities fixed in v15 Read More »

Windows 10 updates and IGSS

Microsoft Windows 10 introduced a new automatic update procedure which compared to previous versions of Windows, did not contain many update settings, basically forcing download and installation of updates on any system connected to the internet. Based on experiences and information shared with the IGSS Support Team, there may be some consequences of the Windows

Windows 10 updates and IGSS Read More »

Windows 10 and IGSS

With the coming release of the Microsoft Windows 10 operating system, system designers and end-users can be expected to start using Windows 10 for their machines running IGSS or at least to set up test environments to verify Windows 10 functionality as well as IGSS compatibility. Please be advised of the following: Softlocks If you

Windows 10 and IGSS Read More »

Scroll to Top