FAQ Question
How can I run an IGSS Silent install?
Answer
- Windows should have the .Net Framework 4.6 installed. That must be done in the Windows “Apps & features” settings
- run the installer VSTO\vstor40.exe add /q to make it quiet
- VCredist\\vcredist_x64.exe /q
- VCredist\\vcredist_x86.exe /q
- VCredist\\vcredist_x86_vs2012_110.exe /q
- msiexec /i vbacore\vbaof11.msi /qb
- msiexec /i vbacore\1033\vbaof11i.msi /qb
- msiexec /i “opc\x64\OPC Core Components Redistributable (x64).msi” /qb
- msiexec /i igss\IGSS.msi /norestart /q
- If you have Excel installed and want to use “custom reports” run
“program files (x86)\common files\microsoft shared\vsto\10.0\vstoinstaller.exe” /i “program files (x86)\schneider electric\igss32\v14.0\gss\rms14.vsto” - “program files (x86)\schneider electric\igss32\v14.0\gss\haspdInst_igss.exe” -install -fi -nomaxosver
- If you want online values in Excel you can run
Windows\Microsoft.NET\Framework\v4.0.30319\regasm IgssExcelRTD.DLL /codebase /tlb - “program files (x86)\schneider electric\igss32\v14.0\gss\dc.exe” /RegServer
- “program files (x86)\schneider electric\igss32\v14.0\gss\def.exe” /RegServer
- “program files (x86)\schneider electric\igss32\v14.0\gss\IGSSopcServer.exe” /RegServer
- “program files (x86)\schneider electric\igss32\v14.0\gss\IGSSopcUAserver.exe” /install /silent