FAQ Question
I have made an RMS template and placed it in a network folder making it available on all stations in my system.
But when I run a report, I get this error:

Answer
This problem occurs because the network folder is not a trusted location in the .NET security settings.
To add your folder to the security settings, run the following command from a command prompt.
C:\WINDOWS\Microsoft.NET\Framework\v2.0.50727\caspol -q -m -ag LocalIntranet_Zone -url “\*” FullTrust -n IGSS32V8_Report
Remember to replace with the network path you’re using.
Example :
C:\WINDOWS\Microsoft.NET\Framework\v2.0.50727\caspol -q -m -ag LocalIntranet_Zone -url “\\10.87.45.32\RMSTemplates\*” FullTrust -n IGSS32V8_Report