Answer
When you’re inside a dialogue in IGSS, you can use the “?” in the upper right corner to get help on the individual field or button in the dialogue. A small popup window with a yellow background will appear, but apparently you cannot do anything with the help contents. Luckily, this is not the case. If you right-click on the popup window, a menu appears.
To print the contents, select “Print”.
“Failed to render the report. Make sure you have a printer defined in your system, and sufficient memory and disk space.”
The solution is to disable the “Run as service process” setting.