Answer
Automatic printing can be accomplished either by using the Job Scheduler program or by using a DOS prompt. See the following.
Detailed intructions for setting up automatic print out of graphs is found in the on-line help file called “Global Help”. Go to the Start button on the Windows desktop, click on Programs, then IGSS32 3.0 and find and open Global Help. Click on the “Index” tab and key in as search criterium “command line interface”. When found, choose “to Supervise”. Read the instructions to choose the parameters that best fit your needs.