Error initializing VBA

FAQ Question

I get the error “Error initializing VBA (hr= 80040562)” when trying to start Definition.

Answer

This error occurs because the dc.exe module is not registrered correctly in Windows Vista when installing IGSS. You can register dc.exe correctly by following this procedure.

  • Log into Windows Vista as an administrator.
  • Open a command prompt.
  • Enter “dc /RegServer” and press Enter.
  • Enter “def /RegServer” and press Enter.

This should register dc.exe correctly and enable you to open Definition without the above-mentioned error message.

Scroll to Top