Number of OP Stations
99 operator stations
In IGSS the maximum number of operator stations that could be connected to an IGSS server was 50. This limit has been increased to 99.
Specify SMTP credentials for e-mailing reports
When using e-mail to send reports it is now possible to specify credentials for the SMTP server connection from the Reports tab in System Configuration.