Design and Runtime modes

You can split all IGSS users into two rough user types– the system designer and the system operator. This is why we’ve invented two modes in the IGSS Master module.

  • The Runtime mode for the monitoring and control tasks
  • The Design mode for the development and design tasks

The number of features available in Design mode is higher than the one in Runtime mode. By using access control, you can block certain users from entering Design mode.