In IGSS V9, the IGSS Reports module replaces the RMS module and the two standard report modules: Snapshot reports and Periodical reports. Previously defined standard reports are still available through the new reports module and existing RMS reports can be converted into IGSS V9 custom report formats.