Calculations
Calculations on object values
In IGSS it is possible to define calculations of one or more process values and show the results on a standard process diagrams. Without any programming it will be possible to combine or evaluate any object value or state available in the system.
All basic arithmetical and logic operators will be available along with a number of function calls to get or compare atom values from objects.
Examples of use
Examples of using the Calculation function would be changing of set points, changing of states on a digital object, initiating events or event activation based on a timer, etc.
Execution occurs independently of operator intervention.
See this help topic for more information.