Alarm Trend Widget
The Alarm Trend widget allows you to get a quick graphical overview of the alarm trends in an IGSS project. Here you can see if the system has a tendency to produce more alarms or longer alarm durations. You will also see an alarm timeline that will give you a historical overview of the alarms in the system. In the alarm data grid, you will see an alarm list showing the specific details for each alarm.

Along with the alarms here represented in the statistical pie, the most frequent, the longest lasting and the active alarms can be shown in the alarm data grid view as well.
It is further possible to see the IGSS objects that are most frequent in alarm, along with those objects that are in alarm for a long time for the period selected.