Materials for download

Here you can find and download the different files used in the IGSS Online Training but also faceplate template file for the Altivar procees ATV600

If you use Schneider Electric hardware, we return the favor by supplying you with some faceplates. This means you will be able to take a shortcut in setting up mimics and plc mapping.

Hardware templates / Faceplates Library / Import groups

To import the template into your IGSS Configuration, do the following.

1. Find and download the relevant zip file matching your hardware below.
2. Unzip the the Template to your installation folder, typically:
C:\Program Files (x86)\Schneider Electric\IGSS32\V13.0\GSS\Templates\
(create the Templates folder if not available)
3. Open Definition and import the .CFG file found in the ZIP.
4. For additional setup instructions read the document supplied with the download.

For now only one hardware template is available.

Supported hardware templates ATV630 and series ATV650 series

IGSS V13 - Altivar Process ATV600.zip - Danish Language

IGSS V12 - Altivar Process ATV600.zip - Danish Language

Scroll to Top