Supervise Enhancements
New option to indicate which server the Operator Station is connected to
In IGSS systems that uses the dual server option; it is now possible to have a color indication in Supervise indicating which server the operator station is currently connected to. This can be used in scenarios where one server is considered a backup server – the color coding of all diagrams in Supervise may be used to indicate to the site operator that he is currently connected to the backup server and not the primary server.

New visual note indication on objects in Supervise
A new “Use marks instead of alarms to indicate object notes” setting in the system configuration alters the display of an IGSS object in Supervise when a note is attached. Instead of the alarm color indication, the object will be marked with a small indicator when a note is attached to the object.