Remote Access Solution
Set up web access for clients in few simple steps
The IGSS Remote Access Solution is a cost-effective web access solution which meets the demands for easy access regardless of time or place and without reducing security requirements.
Installing the remote access software server-side and client-side is simple. Setting up security is also very fast and intuitive. All the client needs is a browser and an ID/Password to get access to the plant’s operator station.
Requirements
A remote access solution with IGSS has the following requirements:
- Plant operator station must have the server version of the remote access software installed for example TeamViewer where a client-version is included in the IGSS Master. Other examples are LogMeIn or GoToMyPC.
- The client must have a web browser installed.
How it works
- The client enters the URL for remote access to the operator station.
- The client logs on to the server.
- The client now takes over control of the remote screen, mouse and keyboard.
- The client has full access to all IGSS features as if he was working on a normal operator station.
Security considerations
To improve security, we recommend doing the following:
- Restrict the client’s permissions in the remote access software, as required.
- Set up a firewall between the web client and the plant operator station.
- Set up User Administration in IGSS.
To automate the login process for the user further:
- On the client, configure that the remote access will Auto-start with Windows.
- Predefine the remote access ID and password. (But do ensure all access to the client station is trusted)