Objects on Map
Benefit:
Operators will be able to find pump stations and other geographically distributed objects using the smartphone.
How to use:
GPS coordinates are added in Supervise by entering the GPS values for the object, or by using the IGSS Mobile at the location of a pump station by pressing the “Save New Object Location” button to store the GPS coordinates.
When GPS coordinates are set for an object in the IGSS software or through the app the coordinates will then be visible in Object Details. You can use the IGSS Mobile App to find the object by locating the object in question in the App, going the Object Details and clicking on the Location field.
A new view with a map is opened, by pressing the map icon to the right in Object Coordinates field. The smartphone navigation app can now be opened and can be used to navigate to the object location.