Define Igss mouse interaction

Interaction Tab

In Definition, the system integrator may now specify what should happen when the end-user clicks a descriptor.

On the new “Interaction” tab it is possible to specify the actions to perform when the end-user either left-clicks, right-clicks or double-clicks a descriptor.

It is also possible to select which diagram, faceplate, graph, or xy-plot should be opened, of the “Open Details…” item from the object context menu in system configuration has been checked. 

Then a system integrator can decide within the interaction tab what details should open when clicked on a connected descriptor.

Scroll to Top