Language Versions
Language support in IGSS
IGSS supports multiple languages in the user interface and in the configuration texts. You can thus create a completely multi-lingual SCADA project where users can select individual languages.
In IGSS, you can select a primary and secondary language (Always English) in the program, System Configuration. In a multiuser system, you can even allow individual operator stations to run different languages.
Language setup
Online change of language
Some IGSS installations have multilingual staff, such as on ships. The operator can change the language online in the IGSS Master while the system is running, whereby language is changed in all the online modules at the operator station.
Languages supported
- Czech CSY
- Danish DAN
- English ENG (default language)
- French FRA
- German DEU
- Icelandic ISL
- Norwegian NOR
- Polish POL
- Spanish ESP
- Swedish SVE