Integration with Windows User Management
IGSS allows you to integrate the IGSS user management with the Windows user management, thus allowing for a single sign-on to the system. For Windows PC that are included in a Windows domain or Active Directory, this makes it possible to have a single and centralized administration of IGSS users and their access rights. For PC’s that utilizes alternate logon methods such as fingerprint scanning or the use of smart cards, this can be used to sign Safe Commands in IGSS as well.

The main features of the Windows User Management integration are:
- Single sign-on to Windows and IGSS
- Centralized user administration when used with a Windows Domain Controller or Active Directory
- IGSS access rights are tied to Windows User Groups
- Biometric sensors may be used to sign Safe Commands