IGSS Dashboard
What is the IGSS Dashboard?
IGSS Dashboard is a new module in the series of monitoring tools included in the IGSS V8 SCADA solution. The IGSS Dashboard module offers the end-users of the industrial systems to create their own personalized process overviews on-the-fly. Furthermore, with the Dashboard module, you will get several new ways of displaying different process data, for example, graphs, LOG, and BCL data may be displayed in one view and be updated automatically.
Possibilities with IGSS Dashboards
The IGSS Dashboard process overview is set up by using a number of widgets. Each widget type will allow you to access and display different data which is useful for monitoring the process. The following widget types are available in the IGSS Dashboard:
- Snapshot widget
Gives you continuously process values for a selected IGSS object - Graph widget
A graphical display of one or several selected IGSS objects - Alarm data widget
Provides statistical KPIs and alarm performance data and it can shows the distribution of alarms by areas or diagrams for a period. - Bar and Pie chart widgets
These widgets can show the analog objects process value, with alarm limits and setpoint if defined on the IGSS object. - Log data widget
Provides you with a list of logged process data for one or more selected IGSS objects - Memo widget
Write yellow notes to remind operators of any important events in the system - Reduced data widget
Shows a list of Base Class(BCL) or Hour-Day-Month(HDM) values for one or more selected objects - Web browser widget
Embed any webpage, for example, the local weather forecast or a remote webcam connection - Audit Trail widget
Keep track of user activity by showing a view from the Audit Trail module
The IGSS Dashboard module is run in a separate window, which is particularly useful in multi-screen solutions. Below is shown an illustration of an IGSS Dashboard.