Alarm Notification Per SMS and E-mail
IGSS features remote alarm notification and handling.
The key features are:
- Configure repeated duty plans on calendars specifically for your plant.
- Configure duty personel for each operator.
- Send critical alarms per SMS or E-mail to on-duty operators.
- Filter alarms on calendars duties, on operators or on the alarm server, to only distribute relevant alarms for the time of day, area, priority etc.
- Operators can acknowledge alarms via SMS.
- Operators can control objects remotely via SMS.
- Distribute alarms from multiple IGSS servers or other SCADA/HMI systems (Via incoming SMS only).
- Control the active duty personel from calendar or operator objects, directly from Supervise.
- Set up a backup Notifier, in case of modem or other errors on the main Notifier.
Notifier is the new generation with a completely new look-and-feel similar to Microsoft Outlook Notifier replaces Winpager a legacy module previously being used by many of IGSS users.
For further details about Notifier, try our Demo example available in the IGSS installation, or read our online help on the topic.