Get your copy of Igss Free 50, our free scada version.
With our free SCADA software you can create a project with full functionality from scratch. It is ideal for OEM's, machine builders and others who would like to automate processes or get an efficient and state of the art replacement for existing Operating Panels.
- Freely define up to 50 objects in an IGSS project and run with full functionality.
- Collect data from the PLCs without any time limit.
- Use one of the +90 PLC drivers.
- Upgrade our free SCADA version anytime to a larger IGSS System.
- Project can run in Demo mode.
- Collect real data.
Also Included: Demo with Pre-Configured Diagrams
IGSS FREE 50 can also be ‘switched’ into Demo mode – which gives you a pre-configured IGSS project including several mimic diagrams from different industries. This gives you a good impression of IGSS functionality in a simulated environment. You can also build a new project from scratch and test it with real PLC data.
- Define up to 1,000 objects in an IGSS project.
- Collect real data for one hour.
- Use one of the numerous PLC drivers supported.
Both systems are ideal for OEM’s, machine builders and others who would like to automate processes or get an efficient and state of the art solution for Operating Panels.
To change the mode, both the project and the license must be changed.
It is done easily by using the IGSS Master module. Find the “Open Project” and the “License” buttons located in the Toolbar and for each select the matching menu points for “IGSS Demo”/”IGSS Free 50”.
Cybersecurity Information
Security Guideline
Read our security recommendations for securing an IGSS SCADA installation.
Security Updates
Make sure to keep the IGSS software updated by running IGSS Update or download updates from here. Also remember to keep the Windows Operating system updated by running Windows Update on a regular basis.