When using the Property Table View form to mass-update multiple descriptors or object properties, you can select adjacent or non-adjacent objects or descriptors in the right pane of the Property Table View form and then edit the property cell values for the first or last row in the selection.
When you press Enter, the cell value entire selection will be updated.
See Also
The Property Table Viewer form
Filter the Property Table View form
Searching the Property Table View form
Update cells in the Property Table View form
Copy and paste values in the Property Table View form