Filter the Property Table View form

You can filter the right pane of the Property Table View form to get a better overview of the displayed properties (cells).

You can specify a filter for each column to reduce the number of objects displayed. Filter conditions will accumulate across the right pane of the form, for example specifying a filter "Pump-A" in the Name column and "0" in the Node column will filter the table to only display atoms from the Pump-A object that are connected to the node number 0.

Filter syntax notes:

To filter column in the Property Table View form

  1. In the left pane of the Property Table View form, navigate to the menu item containing the cells you want to filter.
  2. In the right pane, double-click in the grey Filter row of the column you want to filter the content of or press F2 to open the cell for editing.
  3. In the Filter row cell, enter the text you want to display in the column.
  4. Press the Enter key to apply the filter to the column. Only the characters exactly fulfilling the filter criteria will be displayed.

    The background for entire filter row is displayed in a red color to indicate a filter has been applied.

Clear the filter

You can remove a column filter by double-clicking the filter cell for the column and manually deleting the filter text. You can also select the filter cell and press F2 to edit the contents of the cell and then delete the contents.

To remove all the filters for all the columns, click FilterClear filters.

See Also

The Property Table Viewer form

The Property Table Viewer form

Searching the Property Table View form

Copy and paste values in the Property Table View form

Export Property Table View content