Use this form to gain an overview of the objects, descriptors in a diagram or in an area. You can also gain an overview of the object and descriptor properties as well as update the properties for one or more descriptors.
The object and descriptor properties displayed in the Property Table View form are the same properties that can be accessed in the Object Properties form in the diagram.
The Property Table View form presents all the properties in cells in a table-format. This enables you to gain an overview of the properties, filter the cells as well as change the values of the properties, either individually or by selected cells. Editable cells are displayed with a clear black font while cells that cannot be edited are displayed in a light gray font.
Some object and descriptor properties are only accessible through the Property Table View form, for example the Lockeddescriptor property and the position properties (X,Y coordinates) in the diagram.
You only edit existing objects or descriptor properties in the Property Table View form.
You cannot create new objects or descriptors in the form.
None
In the Definition module:
The Diagram Property Table View form:
The Area Property Table View form
The Alarm Property Table View form:
The Object Template Property Table View form
The Property Table View form is divided into two panes - a small left pane and a larger right pane.
See Also
Searching the Property Table View form
Filter the Property Table View form
Update cells in the Property Table View form
Copy and paste values in the Property Table View form
Export Property Table View content