Create a new graph in a separate window

You can create a new graph window for a stand-alone graph, which is not embedded in a diagram, or edit an existing graph window in the Definition module.

To create a new graph window:

  1. In the Definition module, click GraphCreate to open the Graph Properties form.


  2. In the New Graph Properties form > Window tab:
  3. In the Window Properties group:
  4. (Optional) In the Window Caption group:

  5. (Optional) In the Protection field, select the Protect object you want to assign to the graph window if you want to use IGSS Object Level Protection security feature to restrict operator access to graphs.
  6. (Optional) In the Connect to field, select another graph you want open automatically when this graph is opened.
  7. (Optional) Select the Set as Default check box if you want the graph properties you select for this graph to be used as default, when you create new graphs. You can always adjust the properties.

TIP! You can set the present graph properties as the default parameters for all future graphs by selecting the Set as Default check box.

After you have set up the graph window parameters, you must define the default graph period, colors, chart and interface options plus add signal(s) to display in the graph in the different tabs of the New Graph Properties form. Explore the links below for more information on how to do this.

 

See Also

What is a graph?

Create an Embedded Graph

Set graph properties as default values

Graph Properties Form

Change graph properties

Protect a graph

Delete a graph

Connecting objects to each other

Reference a graph from a symbol

Object Naming Rules