X-Axis Property Menu

Use the X-axis property menu to:

Where do I find it?

In the graph area, right-click the X-axis to open the X-axis property menu. If comparing two periods, right-click the lower X-axis to open the X-axis property menu.

Which and how many items the menu contains depend of the previous selections made.

This menu does not exist for the Embedded Graph Basic, which is operated differently – see separate help page.

Preconditions

Stand-alone Graphs and Operator Graphs must be opened in a graph window. Embedded graphs are permanently displayed as part of a diagram.

Menu help

Menu option

Description
Go Backward

Move the graph period back by the selected period.

Go to Date Specify the date and time and move the graph to the date.
Change Period

Select this option to open the Graph Properties form and change the display period of the graph.

Only the Period tab of the Graph properties form will be accessible.

Compare Periods

Select this option to compare the present graph trend with the graph trend for another period.

The graph area will be divided into two sections, the upper section which can be scrolled individually and the lower section which is scrolled together with the upper section.

Single Period Select this option to revert the graph from a split-sectioned graph used for comparing two graph periods to the original single-period graph.
Properties

Select this option to open the Graph Properties form.

Use the New Graph Properties form to define the graph period, the object atoms and appearance of the graph line, the data source to be displayed in the graph, the graph title and the font properties for all graph texts.

You can also set up the graph legend properties and chart colors as well enable display of the graph toolbar and status bar.

 

See Also

Graph Properties Form

Y-Axis Property Menu

Compare Periods Menu