About positioning and resizing descriptors

You can position and/or re-size a descriptor in the Definition module in three ways:

 

Some descriptors cannot be re-sized using the Property Table Viewer or the Position and Size toolbar, e.g. object symbols and object texts such as object name, state/value, description, atom time stamps and/or Atoms in OPC server.

The screen coordinates in IGSS start in the upper left-hand corner and all object placement coordinates in the diagrams are based on the upper left-hand corner of the object symbol icon.

 

Remember to select and position any additionally displayed object information such as object name, state/value, description, units, atom time stamps and/or Atoms in OPC server when re-positioning a descriptor in order to display object information with the descriptor.

See Also

Keyboard shortcuts

Adjust descriptor size and position using the Position and Size Toolbar

Adjust descriptor position and size using the mouse or keyboard

Adjust descriptor position and size using the Property Table Viewer

Re-size a symbol descriptor